Other Parts Discussed in Thread: LP5569
Hello,
I have some questions about charge pump operation.
I will send you a file with the details of the questions.
I am looking forward to your reply.
Best regads,
Hyodo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have some questions about charge pump operation.
I will send you a file with the details of the questions.
I am looking forward to your reply.
Best regads,
Hyodo
Hi Hyodo,
For Question 1:
When the charge-pump automatic-mode selection is enabled, voltage on the LED current LED sinks LED0 to LED8 are monitored. If the current sinks do not have enough headroom, the charge pump gain is set to 1.5* and remains in 1.5* mode until some condition occurs. 3.2V input voltage maybe high enough for your LEDs on, try to decrease the Vin(not low than 2.5V) and confirm the result.
For Question 2:
A 1uF capacitor is suggested to connected between PGND and VOUT. The charge-pump output capacitor is charged by the flying capacitor every switching cycle (1.25 MHz). This fast switching action requires that a low-inductance and low-resistance capacitor (ceramic) be used and that the output capacitor be connected to the LP5569 VOUT pin with a low-inductance connection. This is done by placing the output capacitor as close as possible to the VOUT and PGND pins of the LP5569 device, with connections on the same layer to avoid vias.
Best Regard
Monet Xu
Hi Monet,
Thank you for your early reply.
About Question 1 , I tried to decrease the Vin(less 3.2V) , I confirmed 1.5x charge pump working.
Thank you.
But thereafter, I tried to increase Vin (~ 4.0 V), but it did not return from 1.5 x mode to 1.0 x mode.
Once it went into 1.5 x mode, it did not return to 1.0 x mode with the LED on(auto mode).
Please let me know how to switch back to 1.0 x mode without LED off.
Best regards,
Hyodo
Hi Monet,
(from your answer.)
When the charge-pump automatic-mode selection is enabled, voltage on the LED current LED sinks LED0 to LED8 are monitored. If the current sinks do not have enough headroom, the charge pump gain is set to 1.5* and remains in 1.5* mode until some condition occurs. 3.2V input voltage maybe high enough for your LEDs on, try to decrease the Vin(not low than 2.5V) and confirm the result.
What conditions are “some condition occurs” in above your comment?
Could you please let me know the condition for transition from 1.5x to 1x when they set the auto mode?
Thanks
Hi Yusuke,
Under described condition, the charge pump gain is set to 1.5x and remains in 1.5x mode until one of the following occurs:
In addition, charge pump return to 1x mode select can also be configurate by cp_return_1x bit in the MISC Register. When set cp_return_1x=1, charge pump mode is forced to 1x mode during shutdown or power save entry.
Best Reagrd
Monet Xu
Hi Monet-san
Regarding #3,
3. The LP5569 device entries power save when the charge pump is in automatic mode(CP_MODE_bits=3h)
Customer found the issue that was not return from 1.5 x mode to 1.0 x mode in Auto mode when they tried to increase Vin(~4.0V).
From your comment in the following E2E session
When setting the registers as the following:
cp_mode=11 ,cp_return_1x=1 ,powersave_en=1
If the VIN voltage drops once and the 1.5x mode is turned on and then the VIN voltage rises due to battery charging, charge pump will return to 1x mode while the LED is lighting.
Could you please let me know the condition that charge pump will return to 1x mode during Auto mode setting.
Also, could you please let me know the reason of customer verification results (not return to 1 x mode)?
Thanks
Muk
Hi Muk,
The comment in the attached E2E session maybe have some unreasonable. I will check on the EVM board and reply to you as quick as possible.
Best Regard
Monet Xu
Hi Yusuke,
I had done some test on the EVM Board and check some documents. Please refer to the following suggestions:
Best Regard
Monet Xu
Monet-san,
Regarding 3. The LP5569 device entries power save when the charge pump is in automatic mode(CP_MODE_bits=3h)
In case of customer set CP_MODE_bits=3h, powersave_en=1, Charge pump will return to x1 mode when All LEDs will be changed to inactive. Is it correct?
Could you please let me know the time between all LEDs turn off and the charge pump changed to x1 mode?
Thanks
Muk
Hi Yusuke,
Yes, When the LED outputs are not active, the LP5569 device is able to enter the power-save mode automatically, thus lowering idle-current consumption down to 10 μA (typical).
The time between all LEDs turn off and charge pump changed to x1 mode is at the millisecond level, and We don‘t provide the precise spec.
Monet Xu
Monet-san,
Thank you for your answer.
Customer is considering the device control method about transition from x1.5 mode to x1.0 mode, if they cannot turn off LED.
From your comment,
Customer will use #2 (forced to x1.0 mode)
(Procedure)
> Auto mode : x1.5 mode (Low Vin)
> Increased Vin : Customer detect the increasing voltage from system.
> They change the charge pump mode to x1.0 mode via the MISC register. (forced x1.0 mode)
> Wait time
> They change the charge pump mode from x1.0 mode to Automatic mode (Customer would like to use the auto mode, basically)
Is this procedure no problem?
Also, could you please your recommendation for wait time between x1.0 mode and Automatic mode?
Thanks
Muk
Hi Muk,
This procedure is feasible. You can also directly try the following steps:
(Procedure)
1. Auto mode : x1.5 mode (Low Vin)
2.Increased Vin : Customer detect the increasing voltage from system.(make sure the increased voltage is high enough to make the auto mode being 1x status )
3. Wait time(Tw)
4.They change the charge pump mode from x1.0 mode to Automatic mode (Customer would like to use the auto mode, basically)
The minimum voltage which can make charge pump being 1x under auto mode can be test on your board and please reserved range for reliability. And at least several hundreds of us should be waiting between mode changed.
Best Regard
Monet Xu
if there is no further feedback I will close this thread.