Can the UCD3138064A control 6 phases interleaved power stages using DPWM0A, DPWM0B, DPWM1A, DPWM1B, DPWM2A, DPWM2B? Please verify if the phase trigger can be used between DPWM0A,0B,1A,1B,etc...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the UCD3138064A control 6 phases interleaved power stages using DPWM0A, DPWM0B, DPWM1A, DPWM1B, DPWM2A, DPWM2B? Please verify if the phase trigger can be used between DPWM0A,0B,1A,1B,etc...
Hello, what is the topology of your power supply?
Regards,
Bosheng
yes, you can control 6 phase interleaved boost converter, each phase will be interleaved by 60 degree. To interleaved DPWM0A and 0B by 60 degree, you can set DPWM0 to multi mode, set event1=0, and set event3=(1/6)*period. The maximum duty cycle will be limited to 83%. The interleave between DPWM0 and DWPM1 is achieved by phase trigger register.