Hello,
Some colleagues recently measured the loop gain on a TPS543B20 based buck converter using five different ramp resistor selections and found 34.8k to be the best in terms of worst case phase margin. However, we would like to understand why this particular ramp resistor is the optimal selection and what it’s role is in the control scheme of the component so that this is not just a trial & error approach to optimization.
The application parameters are as follows:
- Vin = 12 V (10.4 V - 14 V range)
- Vout = 2.5 V
- Iout = 18 A max
- Cout = 230 uF
- L = 400 nH
The results were as follows:
Phase Margin(°margin) |
|||||
Resistor |
None |
23.7k |
34.8k |
51.1k |
78.7k |
14V,18A |
43.99 |
46.7 |
47.7 |
45.7 |
34.3 |
12V,18A |
45.507 |
51.1 |
53.15 |
48.9 |
45 |
10.4V,18A |
47.182 |
53.9 |
55.1 |
58.9 |
54.3 |
14V,8.6A |
41.887 |
49.8 |
51.9 |
52.9 |
50.4 |
12V,8.6A |
43.323 |
53.4 |
56.4 |
58.7 |
55.9 |
10.1V,18A |
46.192 |
56.1 |
59.6 |
64.5 |
65.2 |
Bandwidth |
|||||
Resistor |
None |
23.7k |
34.8k |
51.1k |
78.7k |
14V,18A |
122.9 |
179.2 |
190.1 |
249.6 |
306.8 |
12V,18A |
120.4 |
179.9 |
191.8 |
249.6 |
247.7 |
10.4V,18A |
111 |
161.3 |
172.7 |
215.8 |
230.6 |
14V,8.6A |
152.2 |
142.7 |
149.3 |
184.2 |
209.9 |
12V,8.6A |
147.8 |
144.6 |
154.3 |
189.3 |
249.7 |
10.1V,18A |
134.8 |
133.2 |
139.4 |
171 |
206.2 |
Any clarification would be appreciated.
Thank you,
Nick