Can the TPS7A20 parts be used in parallel?. i.e two in parallel to get 600mA
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the TPS7A20 parts be used in parallel?. i.e two in parallel to get 600mA
thanks
Hi Stephen,
Any LDO can be paralleled with a bit of effort. The TPS7A20 does not have a feedback node or NR pin to connect to, so you are left with using ballast resistors to parallel this device. Here is an App note which may be useful to you.
https://www.ti.com/lit/an/slva250/slva250.pdf
We do have plenty of linear regulators which can supply 600 mA without the added complexity of parallel LDO's. If you want, I can review our catalog of parts for a suitable device if you provide me with a list of key requirements.
Thanks,
- Stephen