This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210: Compensation Loop question

Part Number: TPS40210
Other Parts Discussed in Thread: PMP9334,

I've a requirement for SMPS as below:

Vin range: 30-350V

Vout1: 18V @0.7A

Vout 2: 12V @0.5A

Fsw: 85-100KHz

Topology: Flyback DCM

Isolation: NO

Cout: 56.2uF

I've taken feedback from 18V line using type-2 compensator circuit. I looked at some of the example circuits available on TI reference guides but none of them have the design calc when it comes to feedback loop - I also looked at PMP9334 which is similar application range, but again the feedback loop design calc are missing. 

Below is what I've so far working... I;ve tested at 35V for all the low & high loads for my design requirements - the o/p is very regulated. the circuit seems to work ok up to 100V with 10W output load (on 18V line). After this the transformer starts buzzing a bit and the Isns starts to saturate ... 

I saw another post by one of another user here is it possible to share the compensation tool for everyone ? 

I've attached my compensation ckt snapshot here 

can anyone suggest me any directions?