Other Parts Discussed in Thread: LM5146, LM5164-Q1
Hi everyone!
I've designed a buck converter based on LM5146 IC using webench design. Also I checked the design with the quick start calculator. Input voltage is 15v < Vin < 95v and Vout =12V and it is designed for Iout=1A.
But LM5146 is not working at all. EN/UVLO pin is about 2.5V at 27V input. A 2.2uF cap is connected to VCC pin. VCC pin is presented below. it seems that it is kind of restarting! Is any protection activated?
Vout in this situation is about 2.5V and there is no gate pulses for the mosfets. I've checked the design with the circuits presented by TI. The only difference is in the AGND that i forgot to consider. I mean in my circuit, GND and AGND is the same like typical application example in the datasheet.
Looking forward for any comment.
Thanks.