This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61460: Synchronisation

Part Number: LM61460

Is the possible synchronisation frequency independent from resistor on RT?

For example wth RT=33k2 nominal switching frequency would be 400kHz. Can the oscillator be synchronized to 300kHz or 540kHz?

We want to change the frequency depending on running system application between these values.

Thanks