Other Parts Discussed in Thread: TPS22919-Q1, TPS22919, TPS22918
could you refer the Reverse leakage current of 22918q1 ? thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
could you refer the Reverse leakage current of 22918q1 ? thanks
could you refer the Reverse leakage current of 22919q1 ? thanks
VIN=0, VOUT=3.3V if IOUT have input current? how much?
vin = 0, vout =5.5, iout = ?
Hi User,
TPS22918 and TPS22919 do not have any form of reverse current blocking. This means that the body diode internal to the device can conduct current from output to input in the event that vout is larger than vin in DC conditions. As such, we do not spec any form of reverse leakage. All leakage specs are as attached above.