This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3410-Q1: issues

Part Number: LM3410-Q1
Other Parts Discussed in Thread: LM3410

Hi team,

My customer use LM3410XQMF/NOPB in their project.

But in the test, they met two issues:

1. When Vin=5V, FB Pin is 0.6V and not 0.19V with a backup battery (3.9V charge) connected. The current limit of 50mA was not reached for an unknown reason.

2. When Vin=5V, disconnect the backup battery. The LM3410 consumes approximately 1A of high current and is overheating.

The result we expect is a stable charge current of 50 mA when a backup battery is connected at Vin=5V. When the backup battery is disconnected, the device is automatically protected from high current.


Could you please help give some comments or suggestions on these questions ?

Thank you in advance!

 

 

 

Regards,

Ivy