Other Parts Discussed in Thread: LM61460
Hello,
I'm trying to make a 13.5V with LM61460, but the actual test using the EVM is giving me different results.
I only changed Rt and Rfbb values of the EVM and nothing else.
I started out with the default EVM settings and the Vout was correct. but When I adjusted the Rfbb value to make 13.5V Vout, the EVM is giving me a Vout of near Vin.
Vin | Vout Target | Rt | Rfbb | Actual Vout | Remark |
20V | 5V | 33.2k | 24.9k | 5V | Default Setting, 400kHz switching |
20V | 13.5V | 33.2k | 8k | 19.8V | Adjusted Rfbb value from the WEBBENCH 13.5V output setting |
20V | 13.5V | 10k | 8k | 19.8V | changed switching to 1.29MHz |
20V | - | 10k | 10k | 11.2V | Min Rfbb value that actually changes Vout |
Is 13.5V Vout not possible from 20V Vin?
Best regards
Brian