Part Number: TPS23881
Hi Team,
i have a customer inquire about the followig:
1. Is there a LAYOUT GUIDE?
2. What are the requirements for the Via size indicated in the picture?
3. DRAIN1~8 follow the line to build the width. Can the surrounding signals be separated from the ground or must be cleared?
4. Are there special stacking conditions for 1.6mm board thickness/4-layer PCB?