Hi
What is the size of EVM(UCC28780EVM-02)?
1. Total size of EVM
2. White silk(picture)
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
What is the size of EVM(UCC28780EVM-02)?
1. Total size of EVM
2. White silk(picture)
Thanks
Hello David,
Thank you for your interest in the UCC28780EVM-002.
The board's overall X dimension (long side) is 3.800in (96.52mm).
The board's overall Y dimension (short side) is 2.740in (69.60mm).
The white box X dimension (long side) is 2.370in (60.20mm).
The white box Y dimension (short side) is 1.410in (35.81mm).
Top-side component height is about 0.571in (14.5mm).
PCB thickness is 0.040in (1mm) and bottom side components are less than 3mm height.
The assembly overall Z dimension (not including plastic standoffs) is 0.728in (18.5mm).
Regards,
Ulrich