Dear:
In TPS62130 datasheet, Page 6 shows that VH value TYP is 0.65V, but the min value is 0.9V > typ value 0.65V;however , VL TYP value is 0.45V< max value 0.3V; I could not understand that; does it print wrong ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear:
In TPS62130 datasheet, Page 6 shows that VH value TYP is 0.65V, but the min value is 0.9V > typ value 0.65V;however , VL TYP value is 0.45V< max value 0.3V; I could not understand that; does it print wrong ?
Hi,
Amod will feedback to you on Monday US time.
Thanks,
Lishuang
Hi Amod.
My customer has the same confusion, they want to know if it enabled at 0.85V.
Thanks,
Colin
Hi Colin,
EN voltage should be greater than 0.9V to ensure the device is enabled.
Thanks,
Amod