Other Parts Discussed in Thread: TLV751, TPS7A87
Hi
We are looking to upgrade the max current of the LDO we are using (the LP5907QMFX-3.3Q1 with max 250 mA) with a new one with more current (for example the LP5912).
Is there a similar LDO with a max current of 500 mA (or above) but with a dual output? maybe with an indipendent enable output. From a first search I don't understand if all the dual output are indipendent of if it must be specified even if it has two enable pins.
Thank you