This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24130: LTC4425IMSE ALternative

Part Number: BQ24130
Other Parts Discussed in Thread: BQ25713

Hello,

I am looking for a linear SuperCap charger to replace the LTC4425IMSE. Do we have a similar device?

Vin 5V, Vout max 5.4V, ~2A max current.

Thank you and best regards,

Ambroise

  • Hi Ambroise,

     

    In order to charge supercaps up to 5.4V from a 5V input, a buck-boost charger is needed instead of a linear charger. The BQ25713 can meet your supercap charging requirements, but this device is quite different from the LTC4425 linear charger.

     

    Best regards,
    Angelo