Other Parts Discussed in Thread: BQ24210,
Hello everyone. Preface: i am not an electronics engineer so i may have done something...suboptimal.
I have designed a lipo solar charger using the BQ24210 solar charging IC, and at the same time i wanted to have overdischarge protection so i tried to use the BQ2970.
The charger circuit works as expected, but the problem i am facing is that the battery protection doesn't seem to activate the discharge gate so i dont see any voltage on the output of the system.
I designed the solar charger according to the schematic on the datasheet.
And similarly i integrated the battery protector by referencing the schematic from the datasheet
The Full schematic is the following. The Battery is connected to B+ and B- respectively. the B- becomes the ground of the system.
Cout is 2V so the charge mosfet is active. Dout is 0V. I dont see anything particularly wrong with the schematic, but again, it doesn't work so obviously i am doing a mistake somewhere.
Any ideas?
Double Mosfet
eu.mouser.com/.../SSM6N61NU_datasheet_en_20160831-938862.pdf