Other Parts Discussed in Thread: UCC28810, UCC28051
Hi,
One of my customer wants to design circuit for the below specification.
Input voltage - 24V AC/ DC +/- 10%
Output voltage - 17V/1A
Isolation - 1KV
Also need PFC to improve on AC efficiency.
We are thinking of UCC28811 for the application. Can somebody help with the design document including transformer?
Since, DC voltage also the input option, is it possible to apply DC voltage to PFC flyback circuit?
Mitesh