HI
Inputs from USB C type to 5V, 9V, 12V, 20V 5A. The USB C type input voltage is used by the TPS54331 to secure the output voltage to 5V.
But when I check the datasheet, does the TPS54331 Adjustable Output Voltage Down to 0.8 V, and will it output 5V even if 5V is input?