Other Parts Discussed in Thread: UCC28600, LM5023, UCC24650
Hello:
We have several highly compact designs using UCC287xx family.
One of them currently being tested is UCC28730. We used the Web Bench & the Excel Spreadsheet.
Pl see the attached pdf of the report Web Bench produced.
There is a strange entry for Vout actual which is 18.257 apparently based upon the values used in the divider at VS pin
But Vout itself everywhere else reported is 6.2V.
Web Bench calculates 4*(1+Rfbt/Rfbb) which is 18.257V
This is a bit confusing. Vout is determined by this ratio divided by Na/Ns, in which case it makes sense.
Is this the correct interpretation?
Another thing: Lpm can swing wildly clearly based upon Iout.
What should be then used for setting this inductance?
In our case, we have imposed Iout=300mA which gives Lpm as approx 4mH
An achievable value with gap on the core suggested ( our core has a slightly higher cross-section). But if the real load is 50 mA?
Web Bench will give 23 mH, an impossible value to achieve in this core unless you quadruple turns with Rcs =28 Ohms. Also sounds weird but clearly consistent with Vcs
So shall we set Iout=300mA knowing that we would hardly ever have ICs connected to it will draw that amount of current? ..because the Lpri is achievable with 60T:5T:14T?
Any clarification will be highly appreciated.