Hi Sirs,
My customer used the EVM to do the functional test, they have some questions as below, please help to advise. Thanks!
Q1: At dynamic load test, they got the Vout ripple (Vp-p) up to 1.92V, is it correct? (Test condition: Vin=55V, Vout=12V, load current=1.5A~4A, freq=1kHz)
Q2: They got the light load (6W) efficiency only have 59%, why the TPS23730EVM user guide showed it can get the efficiency up to 71%? Could you please share the test condition?
Q3: At Vin=55V, Vout=12V, loading=5A, they observed the Vout rise curve is not smooth, is it correct? what is the reason that will cause the not smooth curve?
Q4: The EVM user guide showed the PCB drawing and they got the EVM PCBA is different. please release the latest schematics and PCBA drawings.