This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65261-1: About resistance value when output voltage is 5V

Part Number: TPS65261-1

Hello,

I would like to ask you about TPS65261-1.
In the item of data sheet 8.3.1, the recommended resistance values when the output voltage is 5V are R1: 73.2kΩ and R2: 10kΩ.
However, I plan to use a resistor with an accuracy of 0.1% to reduce output voltage variations.
Also, due to the size of the resistor, etc., the resistance value that can be adopted is limited, so I am considering setting it to the following value.

R1: 17.8kΩ and R2: 2.4kΩ

Is it possible to use a value lower than the recommended value as described above?
Are there any concerns?

Best regards,