I am having problems synchronizing the PWM IC UC2825A-EP to an external 120Khz clock frequency. The problem occurs during high and low temperatures (-40 Deg Cent. and +70 Deg Cent.)
The PWM frequency varies from 105Khz to as much as 118Khz around these temperature ranges. The external RC components are 1% tolerance, I am using an NPO capacitor for the CT, and we also tried using a film capacitor as well. The external components are not the cause of these wide frequency variations. I believe that the frequency variations are due to temperature, for the most part, caused by the PWM IC temperature tolerances.
I am using the recommended External sync circuit found the the UC2825 datasheet.
In the datasheet the UC2825A-EP has listed a tolerance of +/-5% for the Oscillator temperature stability and about +/-6% for the initial oscillator accuracy. When the free running oscillator is set to the recommended frequency of 10% to 15% slower than the sync frequency, the tolerances of the free running oscillator in the UC2825 drift out of the window in which it can be sync.
I called a TI App Engineer and he recommended using a different sync circuit (as shown in a TI technical Paper “Converter Synchronization Provides Design Flexibility” by John Bottrill):
This circuit is specifically designed for PWM ICs with integrated CT caps. However the TI App engineer thought that this would work fine for our application using the UC2825 as well (it does not have the integrated CT cap).
Question 1: Will this new circuit be able to sync correctly over the UC2825 frequency variations due to temperature and initial tolerances?
Question 2: What is the min and max frequency tolerance in which this new circuit will still be able to sync to the sync frequency using the UC2825 PWM IC? (Our current circuit won’t sync well below 10% of the sync frequency).
Question 3: In the case of this new design example, the CT-Buffer is the signal output that is used to reset the external SR latch. If I use the UC2825, what is the equivalent signal? (I think it is CLK/LEB pin 4).