Hello,
Can you provide the gerber files for the UCC28600EVM 120W. Can you also provide the dimensions? Was this board designed to pass UL, FCC and CE testing?
Regards,
John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can you provide the gerber files for the UCC28600EVM 120W. Can you also provide the dimensions? Was this board designed to pass UL, FCC and CE testing?
Regards,
John
This EVM was not designed to pass UL, FCC, or CE testing. This evaluation module was laid out with the purpose of allowing customers the opportunity to probe the circuit as a learning tool to evaluate the device and how it behaves in a system. There was no intent to be in any kind of format that would be directly applicable to an end users packaged design.
Dimensions: 10 in. x 4.1 in. x .063 in.
Designed for 120 W laptop battery charger applications
Lisa and Jeff,
Thanks for your responsed. Just what I needed to know.
Regards,
John