Everytime i first attach a battery to the EVM, i need to apply power to the pack terminals to stop the shut down mode. Then the bqEvaluation software always show the remaining SOC is 5% or less. Why? it should be 100% right/?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I will try the reset command but what does the reset button do?
i'm using bq28550's EVM.
And I am using the default chemistry which is ID0100 i think. And i am using CEDV functionality.
Meanwhile, i have already set the parameters like full capacity, design capacity, energy, etc.