Hello,
I am planning a design based on UCD9244 controller along with the CSD95372AQ5M NexFET power stage, similar to PMP6000.1, although with four rails and one phase each vs two rails and two phases each and with the CSD95372AQ5M instead of the CSD96370Q5M as I need the higher power.
I'm trying build the circuit in Fusion Digital Power Designer but there is no option for this parts. I guess I should use the discrete mode and add the parts by myself and create a custom driver, but I would like a little guidance on this, as the datasheet of the CSD95372AQ5M isn't very clear on many of the required options.
Also are there any plans on releasing the PMP6000.1 project files? That would also help a lot.
Thanks in advance,
Michael