Hi,
I found the below description in tps2505 datasheet. Does it mean I have to enable the boost first before enable the LDO? I need to enable the boost and LDO independently. How can I do?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I found the below description in tps2505 datasheet. Does it mean I have to enable the boost first before enable the LDO? I need to enable the boost and LDO independently. How can I do?
Thanks.
Does it mean I have to enable the boost first before enable the LDO? Yes
I need to enable the boost and LDO independently. How can I do? EN is a global disable (EN < 0.7V) for the LDO, USB1, and USB2. When EN > 1V, then ENLDO, ENUSB1, and ENUSB2 are used to independently enable/disable the LDO, USB1, and USB2 respectively.