Hello e2e,
I am looking to power the Keystone 1 (C6655) using the LM10011. The EVM uses the digital version for voltage scaling, but the app note on Keystone 1 mentions I can use either Analog or Digital. Do you have a particular preference for CC6655? Also, the buck that goes with LM10011, I see we did testing with the high current LM21215. In my application, I need only 5A out (maximum, for the most part 3A). The app note again mentions any buck with compatible feedback can be used, so I assume any buck with external compensation. Do you have any suggestions and do you know if any testing was done with lower current bucks?
Thank you very much for your help,
Natallia