I am currently working with a LM317hv and LM137hvqml. How do I hook them in parallel to get 3 amps at +40v and -40 volts output?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am currently working with a LM317hv and LM137hvqml. How do I hook them in parallel to get 3 amps at +40v and -40 volts output?
Hi Michael:
What I am trying to do is from a +/- supply +44.5vdc unregulated (no load). Using a two positive variable voltage regulator get 40vdc @3 amps.
Secondly getting -44.5vdc unregulated (no load). Using a two negative variable voltage regulator get -40vdc@ 3 amps.
I will look at the link.
Thanks,
Victor Morita
Hi MIchael:
I have done alot of research. How about this approach.
+ unregulated ---------------lm317hv------------------(+40volt@1.5amps)
------------------------Gnd
- unregulated ----------------lm317hv -----------------Gnd
-------------------------(-40volt@1.5 amps).
The picture is a positive voltage regulator used as a negative regulator
Hi Michael:
This approach is two separate + power supplies with transformer isolation (floating not tied to chassis gnd). One power supply is the + 40volt source and the second is the -40volt source. The second power supply"s plus is tied to the negative of the first. Thereby creating a new power ground and a + and minus supply. I have taken two lab supplies and hooked up the unit in series with no chassis to minus tie in(floating). Hooked up the two power supplies in series to generate a plus and minus supply. What do you think.