Hello,
I use an LMZ14201H in a certain circuit with the following parameters:
Vin: 16-32V
Vout: 11V
Iout: 600mA (max)
Frequency: 330KHz
For some reason we have a peak of Radiated EMI at 70MHz approximately.
Are there any known issues or solutions?
We had in the past serious problems with conducted noises in low load conditions, due to the DCM/CCM transitions, we solved this problem, but the 70MHz radiated is hard to explain.
Thanks