Hello,
The Voutp-p simulation result of LM43602-Q1, LM43601-Q1 on Webench was about 100mV~120mV.
Is this result correct?
I think that this is error in webench.
If yes, could you please correct the Webench?
If not, please let me know the correct simulation value.
The followings are the simulation input conditions.
(1)
LM43601-Q1
Vin=28V
Vout=12V
Iout=300mA
Optimization Tuning is Highest Efficiency
(2)
LM43601-Q1
Vin=28V
Vout=12V
Iout=600mA
Optimization Tuning is Highest Efficiency
(3)
LM43602-Q1
Vin=28V
Vout=8.7V
Iout=1A
Optimization Tuning is Highest Efficiency
Best Regards,
Ryuji Asaka