Hello.
The request to give more detailed description of behavior of a chip of TPS65640.
We can't startup it yet. Isn't present 2,5V on V25_LX (pin 17) and respectively remaining converters aren't launched.
In what there can be a reason why doesn't appear 2,5V on V25_LX? The chip is new, on VIN (pin 18) is 5V - checked.
Whether if isn't present 2,5V on V25_LX there will be a communication on I2C with a chip?
When it is possible to address through I2C a chip? From what I2C in a chip is powered?
Can exist an example of the working schematic to check whether correctly we made the schematic?
If to connect only VIN, AGND, PGND1, PGND2, PGND2, and V25_LX (pin 17) to V25 (pin 19), and all remaining pins is not connected (to clean remaining elements) whether LDO CONVERTER will work?
With best regards, Dmitriy Sadnikov