Other Parts Discussed in Thread: LMG5200
Hi
i try to operate the LMG5200EVM-02 but there is no output signal.
the output load is resistor of 47 Ohm.
On step 1 : I Connect a Supply to J3 Connector (6V).
On step 2 : I Connect a function generator output to the J5 connector (4MHZ, squre signal, 50%, 6Vp-p).
On step 3 : I Connect a Supply to J1 Connector (30V).
On step 4 : power up Supply to J3 Connector (6V). The D1 diode lights up after the driver bias supply comes up.
On step 5 : turn on the function generator which conected to the J5 connector .
On step 6 : Power up the input supply (30 V). The D2 diode lights up after the input supply is powered up.
when i checked the TP9 and TP10 I see the input signal but there is no signal on output.
Please advise.
Best Regards
Yaron