Hi,
I am designing a 3 phase synchronous buck DC/DC converter with 36 V input voltage and 24 V output voltage. The maximum output power is 5kW.
Here is my question:
1. What is the maximum voltage of PIN COMP when the output voltage does not reach the reference? If I need to limit the maximum output current to 115% of the rated current, how can I limit the voltage of PIN COMP?
2. According to the application diagram in the datasheet, PIN EN/SYNC is connected to nothing. Can PIN EN/SYNC be connected to PIN VIN by a resistor (1k) to enable?
Thank you!