LMZ35003 datasheet says below:
The LMZ35003 requires a minimum input capacitance of 4.4 μF of ceramic type. The voltage rating of input capacitors must be greater than the maximum input voltage. The ripple current rating of the capacitor must be at least 450 mArms.
However, reentry large size as 3216 (50V) is not easy to buy and in the future it has a possibility to be discontinue such size. So my customer is now considering to use 1uF of 1608 size (50V) or 0.47uF of 1608 size (50V). If use such small capacitor what problem could be occurred? Also would like to know what point need to check carefully during evaluation. The customer check the behavior with use 4.4uF and 1uF by the WEBENCH but the result shows no big difference.
The target circuit is:
Input voltage: 37V
Output voltage: 15V
Load current: 2A
Please let me know the expert’s comment.
Best regards,
Izumi Maruyama