Hi,
There is a min value of 22uF for stability in the datasheet of the 3.3V version. Is that a "one size fits all" constraint or are there other conditions for stability using a 10uF capacitance ?
My application has a 3mA current draw with very little AC component, a 6V to 36V input voltage and I can add up to 26Ohm of ESR.
Thank you.