I would like to use TPS61252 on my project but I run into some problems. I want 5v output but output voltage is unstable. I used exactly the same schematic in datasheet. I tried different IC and board but no luck.
Inductor: TDK VLS3015ET-1R0N, 1uH, 58 mOhm, 2A
Input cap: Murata GRM219R60J106KE19D, 10 uF, 6.3V, X5R
Output cap: Samsung CL21A226MQQNNNE, 22uF, 6.3V, X5R
Feedback resistors: 768k, 243k
Input voltage: 4V
Output voltage: Fluctuates between 4v and 6.3v
Feedback pin: Fluctuates between 1.24v and 1.28v
Load current: 100mA
Please help me. Thank you.