Hi, team.
Is the current limit threshold precision of TPS24700 also same in 3.3V?
Is the precision related in the voltage?
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, team.
Is the current limit threshold precision of TPS24700 also same in 3.3V?
Is the precision related in the voltage?
Best Regards,
Hirotsugu,
I see your reason for the question as it isn't specified in the EC table (it is stated as spec'd for +12v). Figure 7 shows the effect of (Vcc range + temp) on a typical unit. The sense amp CM operation is optimized for higher Vcc as you can see +12v and +18v are essentially identical. But 2.5v is only an additional 1% variance from 12v so performance at 3.3v would be expected to be excellent also. For margin, assume additional CL tolerance could be as high as +3% at 3.3v vs the 12v specification for 13% total range in the 6 sigma band at Vcc = 3.3v.
Brian