Other Parts Discussed in Thread: UCC24612-1EVM, CSD18536KCS, CSD18535KCS, UCC24612
Hi all,
UCC25630-1EVM-291 is full wave two Diodes Rect.
Many customer want to change Diodes to SRs.
But UCC24612-1EVM is expensive to buy.
There are board which extension wire from SOT-23.
two CSD18535KCS or CSD18536KCS.
two UCC24612-2DBVT
extension board and wires. and some C, R
I do not want 1ohm resistor.
We needs circuit (cut and connect ) picture.
And caution for which wires should be short ( ? mm length )
Thank you,
H.DOI