Hi team,
I have some question of TPS73601 as below. Especially, load regulation.
1. VFB is 1.198 to 1.21V at Tj = 25 deg. How much the VFB during Tj = -40 to 125 deg? I think 1%.
2. Unit of Load regulation mentioned %/mA. How to define this? For example, if Iout=100mA and Vout is setting 1.23V, ⊿Vout=0.05%. So, the worst case is Vout = 1.23 x (1-0.05%) = 1.218V. Is it correct?
3. How much the ⊿Vout(⊿Iout) load regulation during -40 to 125 deg?
4. Below table 6.5 and figure 1 looks like different. Which is the trust value?
Could you please give me your advice?
Regards,
Yoshi