Hello E2E,
I have a customer who is looking to do the following:
19.2 – 28.8V down to 16V with an output current of around 200mA.
Can they use the LM22674 in this configuration? I am not seeing the max Vout specified in the datasheet, but the see on the selector guideline that it can go up to 37V. But on Webench it is listed as a 5V max for Vout. Can you advise on what the output limit is?
Thanks!
Russell