Other Parts Discussed in Thread: TLC59711
I am running three chains of TLC5947 boards of this design from Adafruit (), each of which is bit banged from an Arduino Nano. After a great deal of research (including from these forums, great resource, thanks!), I have come to understand that the TLC5947 is not meant for rapid changes, so sometimes there is flickering when the LED states are changed.
With the BLANK pin disabled, two of the three chains behave better than expected as can be seen in video1. They fade from nothing to full brightness for red, blue, and green without any discernible hiccup. However, the third chain seems to behave more or less at random. When I enable the BLANK pin, all work as expected with the brief flash of all turning off.I have ordered replacement TLC59711 boards, but would appreciate any insight into this problem! If I could get these boards to behave as the two do in video1, that would be the best case scenario. Also, I realize that there are many possible variables at play here, so if there is any key information that would be helpful, please let me know.
Thank you in advance for your help.