Dear E2E :
I use TPS7A16-Q1 as a power for MCU. and the system load is a motor. When i turn on/off the load, i found the LDO Output Voltage turned off,
and can't recover when the input voltage turned normally.
so i check the input voltage when turn on/off the load, and found the input voltage dropped .
Vavg=20V Vdrop=7V. T<20US.. Waveform and Schematic as follows.
2. so i add a resistor 47 ohm between DI and C1. the Output voltage turn to be normal. the input voltage waveform as follow:
Vdrop=3V.
Question:
1. The reason why the output voltage abnormal, Cause the input voltage drop below the output voltage or not ?
2. Why the output voltage can't recover when the input voltage turn into normal voltage?
3.Can you give me some suggestion for improve my schematic, except add a resistor ?
thanks a lot.