Other Parts Discussed in Thread: TPS51220A-Q1
G'day,
I'm using the TPS51120 as part of the power management solution for an automotive device. The device is powered directly from the battery as follows (VBATT_FILT connects to VIN on the TPS51120):
I hoping for some guidance as to the level of EMI filtering/conditioning required by the TPS51120 in an automotive environment. I have surge/load dump (TPSMC20CA) and reverse polarity (RB088LAM-30TFTR) protection, but feel that some sort of common mode choke should be incorporated (located in the 'gap' in the schematic above). Would this be required for successful/optimal operation of the TPS51120? If not the TPS51120 itself, would the common mode choke (or an alternate filtering methodology) benefit the high/low side MOSFETs attached to the TPS51120?
The device is rated up to 15A, with an external 15A fuse on the power input cable. Any input would be greatly appreciated.
Thanks!