Hi,
If possible we would like to know the output voltage tollerences for LP38693SDX-ADJ/NOPB in the following conditions:
Vin: 5.0V, Vout 1.8V, Iout 20mA, Temp range 0-55degC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
If possible we would like to know the output voltage tollerences for LP38693SDX-ADJ/NOPB in the following conditions:
Vin: 5.0V, Vout 1.8V, Iout 20mA, Temp range 0-55degC
Hi ,
While the output voltage tolerance of LP38693, like most linear regulators, is specified across the full operating temperature range, Figure 15 shows how a 1.8 V output device will typically drift over temperature. You can therefore use LP38693 to estimate your tolerance across your abbreviated temperature range.
Very Respectfully,
Ryan