Other Parts Discussed in Thread: TPS54140
The output of TPS54140A 24->5V circuit shows a large Vout ripple in case of No load.
If there exists a load resister for 20mA current , the above ripple disappears.
The follows are the comparison when I changed the inductance value. The waveform of 4.7uH case is clean, but both 33uH and 100uH cases have 0.2Vp-p ripple (cycle time is greater than 20ms).
I want to know the reason of ripple, because my application needs a small current load ( less than 50mA ) .
Why does the ripple disappear by using a small inductance ?