Other Parts Discussed in Thread: SN6501
We are trying to use the LM5105 to drive two N channel FETS that will control the 50V B+ to the drain of a RF power GAN transistor.
We chose this IC, due to ability to quickly turn on and off our 50V B+ rail.
We would like CW as well as fast pulse control.
We have built the basic circuit shown in the 7.2 functional block diagram of the data sheet.
VDD pin has 12VDC.
The N channel FETS are on a 50VDC rail.
The output between the N channel FETS are loaded with 1K Ohm for testing.
The input pin is manually being switched between open (with the pin internally pulled low), and 5VDC.
What we notice, is that the circuit works fine as long as we keep our 50V rail below about 16V. Above 16V, the circuit fails to work in our CW condition.
1) will this chip perform in a CW condition? (if so what do we need to change?)
2) if not, is there a minimum pulse frequency, width and duty cycle that we need to meet?
3) if this is the wrong part for our application, can you recommend a better product?