Other Parts Discussed in Thread: TMS570LS3137, TPS57160-Q1,
Hi,
In the TPS65381A datasheet it looks like VDD1 (linear regulator capable of 1.2V output for the Hercules) uses an external pass FET with no current or temp monitoring. Thus, it looks like we recommend using VDD6 as a current-limited source for VDD1. Because all the LDO rails feed off VDD6, this leaves 600mA guaranteed for VDD1.
The TMS570LS3137 has a max Vcore draw of 700mA during PBIST.
To get around this current limit, it looks like we use the TPS57160-Q1 to supply vcore in TIDA-01537. Is this recommended from a functional safety perspective? All the safety related functionality seems to live on the TPS65381A, which does not supply or monitor VCORE. Can I bypass the VDD1 regulator and instead use VDD1_SENSE to watch the 1.2V output from TPS57160.