I am going to use TPS54332 in my design, my product will be powered by a battery, the nominal voltage of battery is 10.8V, the cut off voltage of battery is about 6.75V, so the input voltage range of TPS54332 is from 6.75V to 10.8V, the output voltage of TPS54332 will be +5V, my question is: can TPS54332 maintain a stable +5V voltage output within this input voltage range with maximum load current?
Thanks and best regards
Kelvin