Hi,
My customer meets an issue about OCL function of TPS56C215-EVM:
Vin=5V;
Vout=1.8V(R7=20K);
L1=680nH;
Mode:(R5=51K,R4=91K)
When the Load change from 2A to 12A,the OCL waveform is different from the discription of datasheet.(CH1:Iout;CH2:Vin;CH3:Vout):
datasheet: When the output voltage lower at 68% of initial voltage, the UVP is on, and turn off the device after 1ms.
Then after 7ms's hiccup mode, reset the device, and the test waveform didn't show it.
Could you please help me figure out the reason behind? Thanks.
The following two test waveform: CH1:Iout;CH2:Vin;CH3:Vout
This is the waveform of SW pin.