Hi,
I would like to use LM5017 as a fly-buck regulator to generate an isolated 7VDC output. The input voltage to LM5017 is between
12 -24VDC. The output current requirement is around 300mA. Please confirm above requirements can be met using LM5017
and recommend appropriate transformer.
Thanks,
Bob